Tresos79001: tresos_cmd.bat has returned the ExitCode 1 during Validation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Tresos79001: tresos_cmd.bat has returned the ExitCode 1 during Validation

15,690件の閲覧回数
manish_singh
Contributor II

Hi,

I have configured GPT driver, MCU driver and ECUM module using Vector DaVinci Tool. MCU and ECUM are getting generated successfully but GPT is generating error as

"Tresos79001 tresos_cmd.bat has returned the ExitCode 1 during Validation"

All the container and parameter for GPT driver are configured but I am not able to get why the tool is generating Validation error. Can you please support me to resolve the Validation error.

ECUM, GPT and MCU configuration files are attached for reference.

 

ECU: S32K144

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

15,161件の閲覧回数
gowthaman_krish
Contributor II

Thank you so much manish singh

0 件の賞賛
返信

15,161件の閲覧回数
manish_singh
Contributor II

Dear Gowthaman,

Yes, I have resolved the issue.

Since these issue were related to Thirdparty configuration and DaVinci was not able to show the proper validation error, so to view the validation error for Thirdparty we need to use Generation Result option as shown below and after that try to solve the validation error.

pastedImage_1.png

13,197件の閲覧回数
NJ_NXP
Contributor II

Thanks Manish

0 件の賞賛
返信

15,161件の閲覧回数
gowthaman_krish
Contributor II

Hi Manish ,

i am also facing same issue .

did you solved the issue or you have any solution how to solve that issue ?

please provide your update ASAP.

0 件の賞賛
返信

14,494件の閲覧回数
Prashanth_Arun
Contributor I

Hi all and Manish,

 

I am having same tresos.bat exit error. 

But after MCAL third party integration everything seems fine and configuration too. What to be done.

Please help ?

0 件の賞賛
返信