Tresos79001: tresos_cmd.bat has returned the ExitCode 1 during Validation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Tresos79001: tresos_cmd.bat has returned the ExitCode 1 during Validation

15,975 Views
manish_singh
Contributor II

Hi,

I have configured GPT driver, MCU driver and ECUM module using Vector DaVinci Tool. MCU and ECUM are getting generated successfully but GPT is generating error as

"Tresos79001 tresos_cmd.bat has returned the ExitCode 1 during Validation"

All the container and parameter for GPT driver are configured but I am not able to get why the tool is generating Validation error. Can you please support me to resolve the Validation error.

ECUM, GPT and MCU configuration files are attached for reference.

 

ECU: S32K144

Labels (1)
0 Kudos
Reply
5 Replies

15,446 Views
gowthaman_krish
Contributor II

Thank you so much manish singh

0 Kudos
Reply

15,446 Views
manish_singh
Contributor II

Dear Gowthaman,

Yes, I have resolved the issue.

Since these issue were related to Thirdparty configuration and DaVinci was not able to show the proper validation error, so to view the validation error for Thirdparty we need to use Generation Result option as shown below and after that try to solve the validation error.

pastedImage_1.png

13,482 Views
NJ_NXP
Contributor II

Thanks Manish

0 Kudos
Reply

15,446 Views
gowthaman_krish
Contributor II

Hi Manish ,

i am also facing same issue .

did you solved the issue or you have any solution how to solve that issue ?

please provide your update ASAP.

0 Kudos
Reply

14,779 Views
Prashanth_Arun
Contributor I

Hi all and Manish,

 

I am having same tresos.bat exit error. 

But after MCAL third party integration everything seems fine and configuration too. What to be done.

Please help ?

0 Kudos
Reply