Tresos79001: tresos_cmd.bat has returned the ExitCode 1 during Validation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Tresos79001: tresos_cmd.bat has returned the ExitCode 1 during Validation

16,042 次查看
manish_singh
Contributor II

Hi,

I have configured GPT driver, MCU driver and ECUM module using Vector DaVinci Tool. MCU and ECUM are getting generated successfully but GPT is generating error as

"Tresos79001 tresos_cmd.bat has returned the ExitCode 1 during Validation"

All the container and parameter for GPT driver are configured but I am not able to get why the tool is generating Validation error. Can you please support me to resolve the Validation error.

ECUM, GPT and MCU configuration files are attached for reference.

 

ECU: S32K144

标签 (1)
0 项奖励
回复
5 回复数

15,513 次查看
gowthaman_krish
Contributor II

Thank you so much manish singh

0 项奖励
回复

15,513 次查看
manish_singh
Contributor II

Dear Gowthaman,

Yes, I have resolved the issue.

Since these issue were related to Thirdparty configuration and DaVinci was not able to show the proper validation error, so to view the validation error for Thirdparty we need to use Generation Result option as shown below and after that try to solve the validation error.

pastedImage_1.png

13,549 次查看
NJ_NXP
Contributor II

Thanks Manish

0 项奖励
回复

15,513 次查看
gowthaman_krish
Contributor II

Hi Manish ,

i am also facing same issue .

did you solved the issue or you have any solution how to solve that issue ?

please provide your update ASAP.

0 项奖励
回复

14,846 次查看
Prashanth_Arun
Contributor I

Hi all and Manish,

 

I am having same tresos.bat exit error. 

But after MCAL third party integration everything seems fine and configuration too. What to be done.

Please help ?

0 项奖励
回复