Tracing a program that jumps into RAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Tracing a program that jumps into RAM

跳至解决方案
2,423 次查看
GaryOlmstead
Senior Contributor I

Hi --
I am using CW with a 9S08QE128.  The program is jumping into RAM and attempting to execute it.  I have the Profiling and Analysis Tools User Guide, and set up is pretty easy until it's time to enter "Address A" and "Address B".  Normally you click on the beginning and ending code you want to trace, but I want Address A to be address 0x0000 and B to be 0x1000, and the Profiling Guide doesn't have any way to do that.

To recap, on the Debug Configuration screen, I selected "Enable Trace and Profile", "Collect Program Trace",  "Automatically", "Collect Trace Until Trigger", Instruction Execute" and "Instruction Inside Range From Address A to Address B is Executed."

So how can I enter an address that I can't click on?

 

Thanks

Gary Olmstead

 

0 项奖励
回复
1 解答
2,334 次查看
GaryOlmstead
Senior Contributor I

If anyone else has this problem, move to the disassembled code window, scroll to the line you want, and click on it.  Same for the end of trace selection.  If that is documented anyplace, I didn't find it.  I just clicked on everything.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,335 次查看
GaryOlmstead
Senior Contributor I

If anyone else has this problem, move to the disassembled code window, scroll to the line you want, and click on it.  Same for the end of trace selection.  If that is documented anyplace, I didn't find it.  I just clicked on everything.

0 项奖励
回复
2,411 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

I got a little bit lost. Are you using codewarrior? are you using P&E multilink? cyclone?

Would be possible that you give a little bit more information about your problem

 

Have a good day

0 项奖励
回复