Sector Protection Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sector Protection Error

2,009 Views
wangjin
Contributor I

My board is P2040NXN7MMC , Code Warrior 10.5, use flash programmer download bootrom in NOR Flash(S29GL01GP). this is a error happened.

Error is :

Error: Erase failed . Flash driver reports the following error(s): Sector Protection Error.

I don.t know why ? I build SRAM Project.

There is someone can help me ? Please

0 Kudos
Reply
1 Reply

1,838 Views
Pavel
NXP Employee
NXP Employee

Unprotect your Flash using CodeWarrior. See attached file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply