after connecting USB port to CWTAP in device manager in port it is not showing console to use the commands like "netparam"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

after connecting USB port to CWTAP in device manager in port it is not showing console to use the commands like "netparam"

941件の閲覧回数
vasusriram
Contributor II

we are using T1040rdb and codewarrior TAP probe.

we connected USB to probe and our system.

after we connected RJ45 cable to ethernet port of TAP and our system . here led is blinking in orange color.

we check the device manager in that ports . here it is not showing the usb serial port to open the console.

タグ(1)
0 件の賞賛
返信
1 返信

824件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

There are two LEDs in CodeWarrior TAP - "RX/TX" and "RUN/PAUSE"

According to "CodeWarrior TAP Probe User Guide", Sections 5.1 and 5.2:

5.1.1 Transmit/Receive indicator
The (labeled TX/RX) indicates the status of communication between the probe and the network/host as follows:
• The LED is red until the probe boot code starts running.
• The LED flashes orange (1 Hz) during configuration of the network/USB interface.
• The LED flashes green (1 Hz) after network/USB interface has is successfully configured. During firmware
updates, the LED flashes green at a higher frequency (5Hz).

• The LED flashes orange when the CodeWarrior TAP is communicating with the target.
• The LED is unlit if the probe is not powered on.

5.1.2 Run/Pause indicator
The status LED (labeled RUN/PAUSE) indicates the state of the target as follows:
• The LED is off when no target power is detected.

• The LED is green when the target is in run mode.
• The LED is red when the target is in pause mode.
• The LED is orange when the target is in mixed mode.
• The LED is initially unlit and remains so until the TX/RX LED starts flashing.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信