Port pins remains latch at high position when debugger is stopped in Codewarrior 

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Port pins remains latch at high position when debugger is stopped in Codewarrior 

1,255 Views
hemantsindkar
Contributor III

Hi,

 

I am using KEA128 and OpenSDA in my project. I am generating PWM signal on port pin. In debug mode if I stop in debug mode, port pin which is generating PWM signal remains in high state. How to fix this.

Labels (1)
0 Kudos
Reply
1 Reply

1,138 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Hemant,

When it run , do not stop, does the PWM can work well ?

You stop the debug, the project stopped, so there is no problem it remains high or low .

BR

Alice

0 Kudos
Reply