Port pins remains latch at high position when debugger is stopped in Codewarrior 

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Port pins remains latch at high position when debugger is stopped in Codewarrior 

1,261件の閲覧回数
hemantsindkar
Contributor III

Hi,

 

I am using KEA128 and OpenSDA in my project. I am generating PWM signal on port pin. In debug mode if I stop in debug mode, port pin which is generating PWM signal remains in high state. How to fix this.

ラベル(1)
0 件の賞賛
返信
1 返信

1,144件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Hemant,

When it run , do not stop, does the PWM can work well ?

You stop the debug, the project stopped, so there is no problem it remains high or low .

BR

Alice

0 件の賞賛
返信