MULTILINK UNIVERSAL 无法使用

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MULTILINK UNIVERSAL 无法使用

1,338 次查看
damonduan
Contributor I

MULTILINK  UNIVERSAL无法再CW6.2、CW6.3上面使用,之前用的Rev.B能直接使用,现在用的Rev.C不能用了。

标签 (1)
0 项奖励
回复
2 回复数

1,143 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Duan,

I suggest update to the new firmware that was released on Dev,4.

http://www.pemicro.com/downloads/download_file.cfm?download_id=346

USB Multilink Universal Resource CD (10275 KB)

don't forget use firmware updates tool to update the firmware.

for example, if you work with 8/16bit MCU, you need udate firmware to support RS08/S08/S12(X)(Z)/…, see below screenshot:

pastedImage_0.png

If the target is PPC5xxx, choose setting as:

pastedImage_1.png

  Can this help you solve the problem?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,143 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Damon

Please install the latest patch on CW6.3 and update with the latest firmware for Multilink Universal:

http://www.pemicro.com/faqs/faq_view.cfm?id=211

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复