MULTILINK UNIVERSAL 无法使用

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MULTILINK UNIVERSAL 无法使用

1,149件の閲覧回数
damonduan
Contributor I

MULTILINK  UNIVERSAL无法再CW6.2、CW6.3上面使用,之前用的Rev.B能直接使用,现在用的Rev.C不能用了。

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

954件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Duan,

I suggest update to the new firmware that was released on Dev,4.

http://www.pemicro.com/downloads/download_file.cfm?download_id=346

USB Multilink Universal Resource CD (10275 KB)

don't forget use firmware updates tool to update the firmware.

for example, if you work with 8/16bit MCU, you need udate firmware to support RS08/S08/S12(X)(Z)/…, see below screenshot:

pastedImage_0.png

If the target is PPC5xxx, choose setting as:

pastedImage_1.png

  Can this help you solve the problem?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

954件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Damon

Please install the latest patch on CW6.3 and update with the latest firmware for Multilink Universal:

http://www.pemicro.com/faqs/faq_view.cfm?id=211

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信