MQX debugging error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX debugging error

1,698 Views
davidzhou
Contributor V

Hi,

I have Code Warrior 10.6.4.FSL_b06015 license, and MQX4.2 installed with K60 tower.

Now I cannot debug all my previously debug-able projects. If I create new project, it still cannot debug. 

But if I change the debugger setting of OS Awareness to None, then it can debug.

Is this a license issue or some settings are missing?

pastedImage_1.png

Thank you,

David

Tags (2)
0 Kudos
Reply
2 Replies

1,604 Views
davidzhou
Contributor V

I recreated an example, with MQX 4.2. It is able to debug. So it seems not related to MQX. Maybe the project data or settings are corrupted.

Thanks

David

0 Kudos
Reply

1,604 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi David,

So you have solved your problem. Thanks for the updating.

Best Regards

Jennie Zhang

0 Kudos
Reply