MQX debugging error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX debugging error

1,693件の閲覧回数
davidzhou
Contributor V

Hi,

I have Code Warrior 10.6.4.FSL_b06015 license, and MQX4.2 installed with K60 tower.

Now I cannot debug all my previously debug-able projects. If I create new project, it still cannot debug. 

But if I change the debugger setting of OS Awareness to None, then it can debug.

Is this a license issue or some settings are missing?

pastedImage_1.png

Thank you,

David

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,599件の閲覧回数
davidzhou
Contributor V

I recreated an example, with MQX 4.2. It is able to debug. So it seems not related to MQX. Maybe the project data or settings are corrupted.

Thanks

David

0 件の賞賛
返信

1,599件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi David,

So you have solved your problem. Thanks for the updating.

Best Regards

Jennie Zhang

0 件の賞賛
返信