MPC5566EVB BAM bootloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5566EVB BAM bootloader

1,422 次查看
ramazan_toprak
Contributor I

Hi,

I am trying to boot with BAM on CAN driver. I attached that file what I sent via CAN, after that I am trying to connect with PE Micro Multilink Universal Revision D, but it sends messages " Debuger retrying force to background mode". Could you help me, what may be happened ? it seems always BAM aktive, PE micro cannot connect to the MCU!

Best regards,

rtoprak

0 项奖励
回复
1 回复

1,319 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please check CONFIG SWITCH on your EVB? If you loaded the code into the board using CAN bootloader, you have probably switched microcontroller to the serial boot mode and this is the reason, why you cannot connect using debugger.

pastedImage_1.png

For internal boot mode, switch BOOTCFG0 and BOOTCFG1 to 0.

Please see also the link below, which tells, how the image should looks like.

https://community.nxp.com/thread/320166#comment-384300 

Regards,

Martin

0 项奖励
回复