question about KEA128 Setup registers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

question about KEA128 Setup registers

1,437件の閲覧回数
vegetarian1
Contributor III

At beginning, system would run __thumb_startup which is used for initialization of PC. __init_registers() would be invoked in it, and the FDIVLD field of Flash Clock Divider Register for KEA128 is set at the same time in my project. It means that register has been written since the last reset. Obviously, it has nothing to do with my code, because it is too earlier. I don't know what __init_registers() has done. But it doesn't happen in another project. How to avoid this problem?
Thank you for your attention.

タグ(1)
0 件の賞賛
返信
1 返信

1,360件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mike,

You can find the definition of " __init_registers()" under CodeWarrior install:

CW MCU v11.0\MCU\ARM_EABI_Support\ewl\EWL_Runtime\Runtime_ARM\Source\__arm_eabi_init.c


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------