MCU won't erase.  Timeout.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCU won't erase.  Timeout.

1,489 Views
dementeddigital
Contributor II

I'm attempting to program my board with some code using CW 10.6.4 and a Multilink FX, and the device won't erase.  What's the best way to root cause this?

 

I get this:

 

fl::target -lc "LC for Simple Flash"

fl::target -b 0x1ffff000 0x4000

fl::target -v off -l off

cmdwin::fl::device -d "FTMRE_PFlash128RAM16" -o "32kx32x1" -a 0x0 0x1ffff

cmdwin::fl::erase all

Beginning Operation ...   

-------------------------

Performing target initialization ...   

Device FTMRE_PFlash128RAM16   

Erasing .............

Error:  Erase Command Failed.  Operation timeout.

Device FTMRE_PFlash128RAM16   

An invalid preference was passed to the GDI protocol plugin(ARM GDI Protocol Adapter)

Error: Erase Command Failed.Operation timeout.

Labels (1)
0 Kudos
Reply
1 Reply

1,343 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Dan,

to solve your problem, we need to know:

1. your chip part number?

2. create a brand new workspace folder, if you create a new project with wizard, can you download the program to target via CW DEBUGGER?

3. test simple flash based on step2. how does it work?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply