KIT MPXY8300A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KIT MPXY8300A

Jump to solution
3,290 Views
riccardocescato
Contributor I

Hi, I'm using the KIT MPXY8300A but I have many problems with the code.

There is an example in the MPXY8300 firmware user's manual but it doesn't work.

When I put it in CodeWarrior the program doesn't recognize the functions and subroutines ready for this kit as for example:

UINT8_MPXY8300_READ_COMP_ACCEL_X (UINT16 * Data, UINT16 TRaw, UINT8 Avg, UINT8 FilterSelect)

.

The code includes this libriary; "reims_firm_io_ES2.h" but I haven't it and I think the subroutines are implemented in this file.

Who know what I have to do or where can I find this library?

Labels (1)
0 Kudos
Reply
1 Solution
3,136 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi riccardo,

i think attached project should include the file that you need.

=====================================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Jennie

View solution in original post

0 Kudos
Reply
3 Replies
3,137 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi riccardo,

i think attached project should include the file that you need.

=====================================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Jennie

0 Kudos
Reply
3,136 Views
riccardocescato
Contributor I

Thanks very much!

Only as confirmation, how can I create an empty project which those files?

I'm using CodeWarrior 10.6 and when I select a Bareboard Project for MPXY 8300 family I can't find such files.

Or better, how can I create I new project from your project? bucause if I create a new project from existing code it uses only the files in the Source directory and so there are problems with the "hidef.h" library.

thanks.

RC

0 Kudos
Reply
3,137 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

please check thread:

KIT MPXY8300A

0 Kudos
Reply