KIT MPXY8300A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,979件の閲覧回数
riccardocescato
Contributor I

Hi,

I'm using CodeWarrior 10.6 on window 8. I bought a KIT MPXY8300A but I have many problem with the code.

 

When I create a new project for the MPXY8300 family, the program doesn't generate the .h files where the functions described in the datasheet are implemented and

also the .h files for interrupts. In this way I can't write the code for my kit!

 

How can I do to create a new project with all these files??

 

Thank you!

ラベル(1)
0 件の賞賛
返信
1 解決策
2,868件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Riccardo,

the file such as reims_firm_io_ES2.h is not CW system file. this file can not generated by CW automatically.

reims_firm_io_ES2.h is from a demo project, we can use it but CW can't create it.

=====================================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Jennie

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,869件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Riccardo,

the file such as reims_firm_io_ES2.h is not CW system file. this file can not generated by CW automatically.

reims_firm_io_ES2.h is from a demo project, we can use it but CW can't create it.

=====================================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Jennie

0 件の賞賛
返信
2,868件の閲覧回数
riccardocescato
Contributor I

Ok I undestand. So, how can I create a new project from the demo project?

Because I have a problem with the hidef.h file that there isn't inside the project but it uses that file!

0 件の賞賛
返信