KIT MPXY8300A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KIT MPXY8300A

跳至解决方案
3,452 次查看
riccardocescato
Contributor I

Hi, I'm using the KIT MPXY8300A but I have many problems with the code.

There is an example in the MPXY8300 firmware user's manual but it doesn't work.

When I put it in CodeWarrior the program doesn't recognize the functions and subroutines ready for this kit as for example:

UINT8_MPXY8300_READ_COMP_ACCEL_X (UINT16 * Data, UINT16 TRaw, UINT8 Avg, UINT8 FilterSelect)

.

The code includes this libriary; "reims_firm_io_ES2.h" but I haven't it and I think the subroutines are implemented in this file.

Who know what I have to do or where can I find this library?

标签 (1)
0 项奖励
回复
1 解答
3,298 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi riccardo,

i think attached project should include the file that you need.

=====================================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Jennie

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,298 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi riccardo,

i think attached project should include the file that you need.

=====================================================

this answer is for you. if it helps, please click on "correct answer " button. thanks!

Best Regards,

Jennie

0 项奖励
回复
3,298 次查看
riccardocescato
Contributor I

Thanks very much!

Only as confirmation, how can I create an empty project which those files?

I'm using CodeWarrior 10.6 and when I select a Bareboard Project for MPXY 8300 family I can't find such files.

Or better, how can I create I new project from your project? bucause if I create a new project from existing code it uses only the files in the Source directory and so there are problems with the "hidef.h" library.

thanks.

RC

0 项奖励
回复
3,299 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

please check thread:

KIT MPXY8300A

0 项奖励
回复