K40x256 Programming guide, API configuration guide and example code for this controller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K40x256 Programming guide, API configuration guide and example code for this controller

跳至解决方案
4,670 次查看
madhusudankumar
Contributor II

I newly  started working with freescale k40x256 board... I need help in getting the user programming guide for the same which contains various APIs for the programming ..I have few sample codes , but the problem which I am facing is that an API guide would help me in programming myself. Write now I am trying to understand the example code , and it is becoming very tedious. Kindly suggest any manual with API.

 

Thanking you

标签 (1)
标记 (3)
1 解答
4,573 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

from your code you use processor expert. so the "API" you mentioned should refer to pe component method. to check the methods usage, right click on the component, then click on "help on the component". see attached video I made.

does this answer your question?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

5 回复数
4,573 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

normally NXP provide the API document right with the SW package.

for example if you use KSDK1.3 pakage, you will find the API document under

C:\Freescale\KSDK_1.3.0\doc

if you are not working with KSDK, please let me know:

which demo code do you work with? is this NXP produced demo? please point the demo download link thus we can check. thanks!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,573 次查看
madhusudankumar
Contributor II

Respected Madam,

                                  I am using Code Warrior and hence the package doesnot have the necessary API.. In order to just give an idea, I am pasting on the codes to blink the LED.. I need an API pdf which could help me to understand the codes. These codes I got from vendors as test codes so I dont have hyperlink of downloadable link

#include "Cpu.h"

#include "Events.h"

#include "LED1.h"

#include "LED_2.h"

#include "LED_3.h"

#include "LED_4.h"

/* Including shared modules, which are used for whole project */

#include "PE_Types.h"

#include "PE_Error.h"

#include "PE_Const.h"

#include "IO_Map.h"

/* User includes (#include below this line is not maintained by Processor Expert) */

/*lint -save  -e970 Disable MISRA rule (6.3) checking. */

int main(void)

/*lint -restore Enable MISRA rule (6.3) checking. */

{

  /* Write your local variable definition here */

  void *LED1_UData=NULL;

  void *LED1_DData;

  void *LED_2_UData=NULL;

  void *LED_2_DData;

  void *LED_3_UData=NULL;

  void *LED_3_DData;

  void *LED_4_UData=NULL;

  void *LED_4_DData;

  int i=0;

  /*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/

  PE_low_level_init();

  LED1_DData = LED1_Init(LED1_UData);

  LED_2_DData = LED_2_Init(LED_2_UData);

  LED_3_DData = LED_3_Init(LED_3_UData);

  LED_4_DData = LED_4_Init(LED_4_UData);

  if(LED1_DData == NULL || LED_2_DData == NULL || LED_3_DData == NULL || LED_4_DData == NULL)

  {

   while(1);

  }

  for (;;)

    {

   LED1_PutVal(LED1_DData, 1);

   LED_2_PutVal(LED_2_DData, 1);

   LED_3_PutVal(LED_3_DData, 0);

   LED_4_PutVal(LED_4_DData, 0);

   for(i=0;i<=500000;i++);

   LED1_PutVal(LED1_DData, 0);

   LED_2_PutVal(LED_2_DData, 0);

   LED_3_PutVal(LED_3_DData, 1);

   LED_4_PutVal(LED_4_DData, 1);

   for(i=0;i<=500000;i++);

    }

  /*** Don't write any code pass this line, or it will be deleted during code generation. ***/

  /*** RTOS startup code. Macro PEX_RTOS_START is defined by the RTOS component. DON'T MODIFY THIS CODE!!! ***/

  #ifdef PEX_RTOS_START

    PEX_RTOS_START();                  /* Startup of the selected RTOS. Macro is defined by the RTOS component. */

  #endif

  /*** End of RTOS startup code.  ***/

  /*** Processor Expert end of main routine. DON'T MODIFY THIS CODE!!! ***/

  for(;;){}

  /*** Processor Expert end of main routine. DON'T WRITE CODE BELOW!!! ***/

} /*** End of main routine. DO NOT MODIFY THIS TEXT!!! ***/

0 项奖励
回复
4,574 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

from your code you use processor expert. so the "API" you mentioned should refer to pe component method. to check the methods usage, right click on the component, then click on "help on the component". see attached video I made.

does this answer your question?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,573 次查看
madhusudankumar
Contributor II

Thank you madam. The video shared by you was really helpful.. Thanking you once again

0 项奖励
回复
4,573 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

Have a great day,

Jennie Zhang

0 项奖励
回复