Interrupt handling problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interrupt handling problem

ソリューションへジャンプ
1,570件の閲覧回数
fabriziotronci
Contributor I

Hi everybody,

I'm new in this community so I apologize in advance if I'm wrong to make this request.

I'm using a mwct1003 with CodeWarrior and I've a problem with interrupt handling.

I have created a new MCU project selecting the mwct1003. I've set up my module registers (Timer A2) to generate an interrupt and I've seen that the interrupt vector table is managed in MWCT10xx_vector.asm file; the module interrupt flag is asserted correctly but the service routine is not executed.

 

May anyone know if there are any special steps to follow to execute the ISR?

 

Thanks

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,456件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Please check the bit in Interrupt Priority Register for Timer A2, whether the IRQ is disabled? And please also compare its settings with the bit I0-I1 in SR register.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,457件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Please check the bit in Interrupt Priority Register for Timer A2, whether the IRQ is disabled? And please also compare its settings with the bit I0-I1 in SR register.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信