Installing CodeWarrior with no Internet Connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Installing CodeWarrior with no Internet Connection

1,992 Views
meirav
Contributor I

Hi,

Is it possible to install and activate the floating license of CodeWarrior Development Suite for Networked Application on a computer that is not connected to the internet?

 

Thanks,

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,908 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Meiraw,

Yes, you can install and active CW floating license without connected to the internet .

Only need use one computer which connected to internet download the license.dat file .

There is a "Floating License Installation Guide for Windows" , you can refer to :

http://www.nxp.com/files/soft_dev_tools/doc/brochure/FLTLICINSTWINBR.pdf 


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,908 Views
meirav
Contributor I

Thank you Alice. 

Meirav 

0 Kudos
Reply