Installing CodeWarrior with no Internet Connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing CodeWarrior with no Internet Connection

1,905件の閲覧回数
meirav
Contributor I

Hi,

Is it possible to install and activate the floating license of CodeWarrior Development Suite for Networked Application on a computer that is not connected to the internet?

 

Thanks,

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,821件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Meiraw,

Yes, you can install and active CW floating license without connected to the internet .

Only need use one computer which connected to internet download the license.dat file .

There is a "Floating License Installation Guide for Windows" , you can refer to :

http://www.nxp.com/files/soft_dev_tools/doc/brochure/FLTLICINSTWINBR.pdf 


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,821件の閲覧回数
meirav
Contributor I

Thank you Alice. 

Meirav 

0 件の賞賛
返信