How to work with release buttons in MQX and PE?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to work with release buttons in MQX and PE?

跳至解决方案
1,298 次查看
norbertoj
Contributor III


Hi!!!

I have some problems to understand how to get an interruption of two release buttons and call a Task to work with the interruption.

 

I created a GPIO_LDD component with two GPIO Pin in Rising Edge. I used ISR (no DMA).

 

I want to know how these interrupts can be linked to the MQX TASKS Template. I created a task with the name "Buttons_task", and this task sends messages to a Main task (Control Task). I need that buttons_task go to the stack when the button is pressed.

标签 (1)
0 项奖励
回复
1 解答
1,175 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Norberto ,

It is not from the interrupt to call Task , While  it is init interrupt in the TASK .

I recommend you refer to the interrupt demo under MQX:  Freescale_MQX_4_2\mqx\examples\isr\build

There is also PE-mqx demo under CW : CodeWarrior_Examples\Processor_Expert\MQXLite\Kinetis

There is also a GPIO interrupt demo :

How to invoke interrupt in GPIO demo project of mqx for more then one time? 

The attachment is a guide for create MQXLITE project on CW with PE, it is the same with MQX .

Hope it helps

Alice

在原帖中查看解决方案

2 回复数
1,176 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Norberto ,

It is not from the interrupt to call Task , While  it is init interrupt in the TASK .

I recommend you refer to the interrupt demo under MQX:  Freescale_MQX_4_2\mqx\examples\isr\build

There is also PE-mqx demo under CW : CodeWarrior_Examples\Processor_Expert\MQXLite\Kinetis

There is also a GPIO interrupt demo :

How to invoke interrupt in GPIO demo project of mqx for more then one time? 

The attachment is a guide for create MQXLITE project on CW with PE, it is the same with MQX .

Hope it helps

Alice

1,175 次查看
norbertoj
Contributor III

Thank you, I could establish the interrupt.

0 项奖励
回复