Hello Norberto ,
It is not from the interrupt to call Task , While it is init interrupt in the TASK .
I recommend you refer to the interrupt demo under MQX: Freescale_MQX_4_2\mqx\examples\isr\build
There is also PE-mqx demo under CW : CodeWarrior_Examples\Processor_Expert\MQXLite\Kinetis
There is also a GPIO interrupt demo :
How to invoke interrupt in GPIO demo project of mqx for more then one time?
The attachment is a guide for create MQXLITE project on CW with PE, it is the same with MQX .
Hope it helps
Alice