How to buy codewarrior basic perpetual with node locked dongle

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to buy codewarrior basic perpetual with node locked dongle

1,644 次查看
wallywillemse
Contributor I

How to purchase codewarrior basic with Processor expert, version 10.7 or thereabouts, perpetual license but node locked through a dongle?

Wally e-mail: [email protected] or cell: (858) 663 5772. 

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,522 次查看
TomasPaez
NXP Employee
NXP Employee

Check the following link on the cost of the CodeWarrior suite, There are 3 options, BASIC , STANDARD and PRO. If you need to use Processor Expert, the PRO is the option with all PE components.

http://www.nxp.com/products/software-and-tools/software-development-tools/codewarrior-development-to...

Dongle use, can be avoided since the license system allows you to move between station by updating the host information.

CWH-DONGLE is the part number you can get in case this is needed. Hope this helps.

0 项奖励
回复

1,523 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Wally,

To order a dongle-based license, order the node-locked option for your CodeWarrior suite and also order the USB licensing dongle (CWH-DONGLE).

Refer to your requirement choose CodeWarrior suite :

CodeWarrior Embedded Software Development Tools|NXP 


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复