Hi Larry,
CW for MCU v10.3 is little old one.
MCU V10.6 is the last version released some months ago.
The MK22FX512 is supported by this version.
With the Project wizard you can create an example with MQX-Lite too.
Regarding MQX V4.1 there is a patch for MK22FN but not for the MK22FX.
Attached you will find the MQXLite doc included in the MCU V10.6 installation.
I don't have anymore the MCU V10.3 installation.
However I've the MCU V10.5.
In the release note I see the following:
New device support:
Kinetis E Series: MKE02Z16, MKE02Z32, MKE02Z64
Kinetis K Series: MK21FX512, MK21FN1M0, MK22FX512, MK22FN1M0.
The MK22FX was included since MCU V10.5
If you need more info regarding MQX, can I suggest you to post a question on MQX Software Solutions
Have a great day,
Pascal Irrle
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------