How to add Processor Expert into my project?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to add Processor Expert into my project?

跳至解决方案
2,056 次查看
aaronlee
Contributor V

I have download GenericBitIO_1.060.PEupd and import to CodeWarrior v10.7

Import_Component_GenericBitIO_Installed.png

I close/re-open my project, that has not any change. 

CommunityEdition.png

How to use GenericBitIO in my project?

标记 (2)
0 项奖励
回复
1 解答
1,735 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Aaron,

Do you want to add Processor Expert into bare board project (without Processor Expert) ?

If yes, please refer to: Adding Processor Expert to C Project (without SDK in PEx Driver Suite)  

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,736 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Aaron,

Do you want to add Processor Expert into bare board project (without Processor Expert) ?

If yes, please refer to: Adding Processor Expert to C Project (without SDK in PEx Driver Suite)  

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------