How to add Processor Expert into my project?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add Processor Expert into my project?

ソリューションへジャンプ
2,045件の閲覧回数
aaronlee
Contributor V

I have download GenericBitIO_1.060.PEupd and import to CodeWarrior v10.7

Import_Component_GenericBitIO_Installed.png

I close/re-open my project, that has not any change. 

CommunityEdition.png

How to use GenericBitIO in my project?

タグ(2)
0 件の賞賛
返信
1 解決策
1,724件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Aaron,

Do you want to add Processor Expert into bare board project (without Processor Expert) ?

If yes, please refer to: Adding Processor Expert to C Project (without SDK in PEx Driver Suite)  

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,725件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Aaron,

Do you want to add Processor Expert into bare board project (without Processor Expert) ?

If yes, please refer to: Adding Processor Expert to C Project (without SDK in PEx Driver Suite)  

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------