HIWAVE MCU speed question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HIWAVE MCU speed question

972件の閲覧回数
simo
Contributor I

Hello all,

 

I have a P&E multilink Universal programmer. I am using MC9s12c µP with 8MHz clock. What should be MCU speed in Flash page? I have always 1.41MHz even I have 8MHz clock. Is my clock dead or do I have to set some settings somewhere? Scope shows nice 8MHz.

 

Should I do anything else than set CLKSEL = 0x00; in SW?

 

This happened now with 4 different µP. Problem in Multilink firmware?

ラベル(1)
0 件の賞賛
返信
1 返信

915件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

You're using P&E Multilink Universal interface.

The last version is Rev C.

I don't know if this can help but a new firmware version has already solved problem with this interface under MCU V10.6 Update4 (Eclipse) and on CW for MCF V7.2 (Classic).

Please have a look to the post:

    Problem with Multilink Rev C - not running after MCU V10.6 Update4 installed & CW for MCF V7.2


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信