HIWAVE MCU speed question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HIWAVE MCU speed question

975 Views
simo
Contributor I

Hello all,

 

I have a P&E multilink Universal programmer. I am using MC9s12c µP with 8MHz clock. What should be MCU speed in Flash page? I have always 1.41MHz even I have 8MHz clock. Is my clock dead or do I have to set some settings somewhere? Scope shows nice 8MHz.

 

Should I do anything else than set CLKSEL = 0x00; in SW?

 

This happened now with 4 different µP. Problem in Multilink firmware?

Labels (1)
0 Kudos
Reply
1 Reply

918 Views
trytohelp
NXP Employee
NXP Employee

Hi,

You're using P&E Multilink Universal interface.

The last version is Rev C.

I don't know if this can help but a new firmware version has already solved problem with this interface under MCU V10.6 Update4 (Eclipse) and on CW for MCF V7.2 (Classic).

Please have a look to the post:

    Problem with Multilink Rev C - not running after MCU V10.6 Update4 installed & CW for MCF V7.2


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply