Error 1722 when installing CodeWarrior MPC5xx edition, v8.7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error 1722 when installing CodeWarrior MPC5xx edition, v8.7

1,146件の閲覧回数
akomarnitsky
Contributor I

Has anyone had similar problem and what should I do?

 

35863_35863.pngpastedImage_1.png

ラベル(1)
0 件の賞賛
返信
1 返信

1,057件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Amir,

What is the Windows OS used ?

Did you try to reload the installer from the web a second time ?

    just to be sure the file was not corrupted.

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信