Error 1722 when installing CodeWarrior MPC5xx edition, v8.7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error 1722 when installing CodeWarrior MPC5xx edition, v8.7

1,149 Views
akomarnitsky
Contributor I

Has anyone had similar problem and what should I do?

 

35863_35863.pngpastedImage_1.png

Labels (1)
0 Kudos
Reply
1 Reply

1,060 Views
trytohelp
NXP Employee
NXP Employee

Hi Amir,

What is the Windows OS used ?

Did you try to reload the installer from the web a second time ?

    just to be sure the file was not corrupted.

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply