Development environmnet for K21_LK5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Development environmnet for K21_LK5

1,164件の閲覧回数
gangriver
Contributor I

New to kinetis and need to do a quick project with K21_LK5. For the development environment, I will need a multilink interface and (maybe a free version since it will be below 64k) CodeWarrior® for MCUs (Eclipse IDE), right? Or, an IDE from IAR? Any comments are greatly appreciated!!!

ラベル(1)
0 件の賞賛
返信
1 返信

1,082件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Gary,

you use K21 I suggest you use KDS3.2 which is a free SW without code size limitation

Kinetis Design Studio Integrated Development Environment (IDE)|NXP 

or you can also use CW10.7

CodeWarrior for Microcontrollers-Eclipse IDE|NXP 

the CW special edition (free version) has 64KB code and data size limit for Kinetis E,L,M Series

for more information, see http://cache.nxp.com/files/soft_dev_tools/doc/fact_sheet/950-00437.pdf


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信