Development environmnet for K21_LK5

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Development environmnet for K21_LK5

773 次查看
gangriver
Contributor I

New to kinetis and need to do a quick project with K21_LK5. For the development environment, I will need a multilink interface and (maybe a free version since it will be below 64k) CodeWarrior® for MCUs (Eclipse IDE), right? Or, an IDE from IAR? Any comments are greatly appreciated!!!

标签 (1)
0 项奖励
回复
1 回复

691 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Gary,

you use K21 I suggest you use KDS3.2 which is a free SW without code size limitation

Kinetis Design Studio Integrated Development Environment (IDE)|NXP 

or you can also use CW10.7

CodeWarrior for Microcontrollers-Eclipse IDE|NXP 

the CW special edition (free version) has 64KB code and data size limit for Kinetis E,L,M Series

for more information, see http://cache.nxp.com/files/soft_dev_tools/doc/fact_sheet/950-00437.pdf


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复