Codewarrior tap can not connect to the board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior tap can not connect to the board

1,714 Views
hxmh
Contributor I

Hello,i am using a new codewarrior tap,the board i am using is P1010,the codewarrior version i am using is 10.5.But,the codewarrior tap can not connect to the board,the errors show as the pics.Can you help me to solve the problem?Thank you!

63545_63545.JPG1.JPG63546_63546.JPG2.JPG63547_63547.JPG3.JPG63548_63548.JPG4.JPG63549_63549.JPG5.JPG

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,600 Views
trytohelp
NXP Employee
NXP Employee

Duplicated post with Codewarrior tap status wrong

0 Kudos
Reply

1,600 Views
hxmh
Contributor I

Yes, the codewarrior version i used is 10.5.The probe i used is JTAG /COP probe has a 16-pin connector.I did as the demo told,but it had the error as i described.Can you tell me what should i do next?Thank you!

0 Kudos
Reply