Codewarrior tap can not connect to the board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior tap can not connect to the board

1,670件の閲覧回数
hxmh
Contributor I

Hello,i am using a new codewarrior tap,the board i am using is P1010,the codewarrior version i am using is 10.5.But,the codewarrior tap can not connect to the board,the errors show as the pics.Can you help me to solve the problem?Thank you!

63545_63545.JPG1.JPG63546_63546.JPG2.JPG63547_63547.JPG3.JPG63548_63548.JPG4.JPG63549_63549.JPG5.JPG

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,556件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Duplicated post with Codewarrior tap status wrong

0 件の賞賛
返信

1,556件の閲覧回数
hxmh
Contributor I

Yes, the codewarrior version i used is 10.5.The probe i used is JTAG /COP probe has a 16-pin connector.I did as the demo told,but it had the error as i described.Can you tell me what should i do next?Thank you!

0 件の賞賛
返信