Codewarrior/Kinetis design studio and plantuml integration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior/Kinetis design studio and plantuml integration

1,279件の閲覧回数
preethimahadeva
Contributor I

Has anyone successfully installed the plantuml plugin for Eclipse in Codewarrior/Kinetis design studio? Even after the plugin installation, I don't see the option in Windows->Show View.  When I try to update the plugin, it tells me there are dependencies that can't be resolved.  

0 件の賞賛
返信
1 返信

1,115件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Preethi,

I have not used plantuml on CodeWarrior or KDS, but it should work if the plug in supports the eclipse version used as base for the IDE. How did you installed the plugin? make sure you followed this guide:

Integration with Eclipse 

You could also check the plantuml Questions & Answers page and see if someone has encountered the same issues:

PlantUML Q&A 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信