Codewarrior/Kinetis design studio and plantuml integration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior/Kinetis design studio and plantuml integration

1,275 Views
preethimahadeva
Contributor I

Has anyone successfully installed the plantuml plugin for Eclipse in Codewarrior/Kinetis design studio? Even after the plugin installation, I don't see the option in Windows->Show View.  When I try to update the plugin, it tells me there are dependencies that can't be resolved.  

0 Kudos
Reply
1 Reply

1,111 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Preethi,

I have not used plantuml on CodeWarrior or KDS, but it should work if the plug in supports the eclipse version used as base for the IDE. How did you installed the plugin? make sure you followed this guide:

Integration with Eclipse 

You could also check the plantuml Questions & Answers page and see if someone has encountered the same issues:

PlantUML Q&A 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply