Codewarrior 6.3 license error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior 6.3 license error

1,631 Views
kameliabakiri
Contributor I

Dear support team,

 

Currently I m trying to set up my Codewarrior 6.3 / 6.4 and I have an issue with license.

When I use CW v 6.3 I have a message that says " Unable to use the plugin ' Embedded Coldefire Linker". It is licensed and a valid license key was not find.....

 

And with CW v 6.4 the binary files are not generated when I hit "make" it seems like the compiling is done but not the files linking.

For both of them I tried the 3 types of licenses :

- Dongle

- Ethernet node locked

- Disk node locked

 

Please could you provide any support for the issue ?

 

Thank you in advance.

 

Regards,

 

Kamelia Bakiri

 

Firmware Engineer - Schlumberger

Labels (1)
0 Kudos
Reply
1 Reply

1,394 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Kamelia Bakiri,

from your question, your CW can't recognize your license.dat file.

some customers have this problem because of the environment variable setting:

pastedImage_0.png

check if the LM_LICENSE_FILE path includes the license.dat of Codewarrior, please suppress following environment variable: LM_LICENSE_FILE in the right path. The  environment variable can be setting by click "start", "settings", "control panel", "system", "Advanced", "environment variable". (See attached screenshot) the LM_LICENSE_FILE should be something like: {your CW install}\license.dat

if the problem can not be solved, more information is needed from you:

1. your CW version:  Start the IDE and click on Help | About Freescale CodeWarrior. Click on Installed Products.Save all info displayed into a txt file.

2. your license.dat file

your license file is your personal asset, please don't share it here in public.

I suggest you send above information to NXP support by submitting a case:

How to submit a new question for NXP Support


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply