CodeWarrior for MPC5744P?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior for MPC5744P?

1,168件の閲覧回数
jaureshsieh
Contributor II

i need CodeWarrior for MPC5744P?

which time that can got the CodeWarrior for MPC5744P?

ラベル(1)
0 件の賞賛
返信
1 返信

1,044件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

Unfortunately MPC57xx family  is not officially supported by CodeWarrior.

At this time there is no plan to support this family.

We're supporting:

     - MPC55xx and some MPC56xx via CW for MPC55xx/56xx V2.10,

     - MPC56xx via CW for MCU V10.6.4 (+ Patch V10.6.5)

For MPC57XX, it is recommended to use a 3rd party e.g.  Multi by GHS (Green Hills Optimizing Compilers)

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信