CodeWarrior for MPC5744P?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior for MPC5744P?

1,211 Views
jaureshsieh
Contributor II

i need CodeWarrior for MPC5744P?

which time that can got the CodeWarrior for MPC5744P?

Labels (1)
0 Kudos
Reply
1 Reply

1,087 Views
trytohelp
NXP Employee
NXP Employee

Hi,

Unfortunately MPC57xx family  is not officially supported by CodeWarrior.

At this time there is no plan to support this family.

We're supporting:

     - MPC55xx and some MPC56xx via CW for MPC55xx/56xx V2.10,

     - MPC56xx via CW for MCU V10.6.4 (+ Patch V10.6.5)

For MPC57XX, it is recommended to use a 3rd party e.g.  Multi by GHS (Green Hills Optimizing Compilers)

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply