CodeWarrior comple link question(Error -1073741811)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior comple link question(Error -1073741811)

3,050件の閲覧回数
DerekXiang
Contributor I

Hi, All,

My Compile environment is CodeWarrior 11.1 + Updates3. Computer systerm is Windows10.

Error information is the following:

**** Build of configuration FLASH_SDM_LPM for project 56F81768_HBLLC ****

"D:\\Freescale\\CW MCU v11.1\\gnu\\bin\\mingw32-make" -j8 all
'Building target: 56F81768_HBLLC.elf'
'Executing target #25 56F81768_HBLLC.elf'
'Invoking: DSC Linker'
"D:/Freescale/CW MCU v11.1/MCU/DSP56800x_EABI_Tools/command_line_tools/mwld56800e" -o "56F81768_HBLLC.elf" @@"56F81768_HBLLC.args"
mingw32-make: *** [56F81768_HBLLC.elf] Error -1073741811

I clean this project and re-compile it. The error information is same. Then I build a new default project, and compile it, but the error information is same yet (mingw32-make: *** [xxxxxxx.elf] Error -1073741811). Then I re-install codewarrior 11.1+update3, the error information is same.

How to settle it? Hope to your help. Thanks!

0 件の賞賛
返信
2 返答(返信)

2,460件の閲覧回数
tsairo
Contributor I

This morning, the command line tools of CW for MCU 10.6.4 started giving this exact same error code. At first glance I thought something changed in my Windows installation to disturb Make, but I noticed that even calling the compiler binary without any arguments gives the same error. It does not print anything to stdout, regardless of any command line arguments.

C:\>"C:\Freescale\CW MCU v10.6.4\MCU\PA_Tools\Command_Line_Tools\mwcceppc.exe"

C:\>echo %ERRORLEVEL%
-1073741811

Any ideas to fix this? Maybe this is related to license manager?

EDIT: Reinstalling Codewarrior does not fix the problem. Also, at least in my case mwcceppc.exe is broken but mwasmeppc and mwldeppc do seem to work:

C:\>"c:\Freescale\CW MCU v10.6.4\MCU\PA_Tools\Command_Line_Tools\mwasmeppc.exe"

Freescale Assembler for Embedded PowerPC.
Copyright(C) 2013, Freescale Semiconductor, Inc.
All rights reserved.
Version 4.3 build 285
Runtime Built: Aug 28 2014 13:11:02

Usage: mwasmeppc.exe [-options]... [files]... [[@]@response]...

Please enter 'mwasmeppc.exe -help' for information about options.

 

 

0 件の賞賛
返信

2,939件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI Derek

Does this problem only exist in CodeWarrior 11.1 + Updates3? does it happen in CodeWarrior 11.1 only?

This problem is in a specific demo code ?  or all project?

Thanks,

Jun Zhang

0 件の賞賛
返信