Chip reported error during erase

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Chip reported error during erase

3,930件の閲覧回数
stive
Contributor I

hello

i just try to erase my project and a faced by a Error of erase failed

I am not sure but I thinks it is something related to the ram problem

dose anybody know how could I should solve the problem?

hanks 

ラベル(1)
0 件の賞賛
返信
7 返答(返信)

3,731件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Stive.

what chip do you work with?

Best Regards,

Zhang Jun

0 件の賞賛
返信

3,731件の閲覧回数
stive
Contributor I

Hi ZhangJennie

and thanks for your reply

I use MPC555

0 件の賞賛
返信

3,731件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi Stive,

Can you please specify which board are you using? Is it a Freescale EVB? Are you targeting internal Flash memory?

Could you possibly post your Flash Programmer Target Configuration dialog screenshot and Console Log?

Which configuration file (.cfg) do you use to initalize your board?

Stanislav

0 件の賞賛
返信

3,731件の閲覧回数
stive
Contributor I

Hi stanislav

thanks for your reply

I'm using the board which is provide for our project

it is designed by one of our teammate

we are not using the EVB

Best regards

stive

0 件の賞賛
返信

3,731件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi stivie,

I've successfully tested erase and blank check of the internal flash of MPC566EVB.

see my target configuration screenshot:

CWMPC5xx_Flash_Programer.png

It uses internal SRAM buffer. so it should work without the External SRAM on your board.

At which address the blank check fails? perhaps the number Flash programing cycles (at 0x8000) has been reached, so you are unable to reprogram it..

Can you possibly try to create an empty bareboard project for MPC555 build it and try to flash it?

Hope it helps.

Stan

0 件の賞賛
返信

3,731件の閲覧回数
admin
Specialist II

Hi Stive, could you please share the details on which Freescale device are you using.

0 件の賞賛
返信

3,731件の閲覧回数
stive
Contributor I

Hi there and thanks for your reply

I use CW8.7 and

The error occur when I tried to do programming by using flash programming

In this case I have some problems

1st in the case of blank check I faced by error:

Fail reading mismatch address

And then connection failed

2nd in the case of program and verify when we do verify it said:

Data Mismatch at address: 0x00008000 Expected: 0x48 Actual: 0x00 


i guess it is maybe is related to the ram addressing or something which is related to

thanks for your help

Best

Stive

0 件の賞賛
返信