Change the MCU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Change the MCU

跳至解决方案
2,047 次查看
pascalschröer
Contributor V

Hi,

 

is it possible to change the uC in a project? I would like to change the processor from

MK20DX128VLH5 to MK10DX128VLH7. I'm using CW1.6 and no PEX

 

Thanks

标签 (1)
0 项奖励
回复
1 解答
1,954 次查看
trytohelp
NXP Employee
NXP Employee

Hi Pascal,

You're using CW for MCU V10.6.

You've created a project for MK20DX128VLH5 without Processor Expert.

With Processor Expert you can easily change the processor.

Now without processor expert I think the best way is to create a new project for MK10DX128VLH7 and to add your sources files.


Have a great day,
Pascal

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,955 次查看
trytohelp
NXP Employee
NXP Employee

Hi Pascal,

You're using CW for MCU V10.6.

You've created a project for MK20DX128VLH5 without Processor Expert.

With Processor Expert you can easily change the processor.

Now without processor expert I think the best way is to create a new project for MK10DX128VLH7 and to add your sources files.


Have a great day,
Pascal

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复