Change the MCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,123件の閲覧回数
pascalschröer
Contributor V

Hi,

 

is it possible to change the uC in a project? I would like to change the processor from

MK20DX128VLH5 to MK10DX128VLH7. I'm using CW1.6 and no PEX

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
2,030件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Pascal,

You're using CW for MCU V10.6.

You've created a project for MK20DX128VLH5 without Processor Expert.

With Processor Expert you can easily change the processor.

Now without processor expert I think the best way is to create a new project for MK10DX128VLH7 and to add your sources files.


Have a great day,
Pascal

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,030件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Pascal,

You're using CW for MCU V10.6.

You've created a project for MK20DX128VLH5 without Processor Expert.

With Processor Expert you can easily change the processor.

Now without processor expert I think the best way is to create a new project for MK10DX128VLH7 and to add your sources files.


Have a great day,
Pascal

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信