Change the MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change the MCU

Jump to solution
2,040 Views
pascalschröer
Contributor V

Hi,

 

is it possible to change the uC in a project? I would like to change the processor from

MK20DX128VLH5 to MK10DX128VLH7. I'm using CW1.6 and no PEX

 

Thanks

Labels (1)
0 Kudos
Reply
1 Solution
1,947 Views
trytohelp
NXP Employee
NXP Employee

Hi Pascal,

You're using CW for MCU V10.6.

You've created a project for MK20DX128VLH5 without Processor Expert.

With Processor Expert you can easily change the processor.

Now without processor expert I think the best way is to create a new project for MK10DX128VLH7 and to add your sources files.


Have a great day,
Pascal

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,948 Views
trytohelp
NXP Employee
NXP Employee

Hi Pascal,

You're using CW for MCU V10.6.

You've created a project for MK20DX128VLH5 without Processor Expert.

With Processor Expert you can easily change the processor.

Now without processor expert I think the best way is to create a new project for MK10DX128VLH7 and to add your sources files.


Have a great day,
Pascal

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply