CYCLONE使用问题

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CYCLONE使用问题

1,642 次查看
ningbozhh
Contributor I

我们使用的是飞思卡尔 9S12VR32号9S12VR64芯片,在使用CYCLONE Programmers时,找不到正确对应的芯片:

CYCLONE中有9S12VR32_1x16x16k_16k  和 9S12VR32_1x16x256_512_b  而实际的9S12VR32是32kFlash_512bEEPROM.  SAP 创建Image时,两种VR32芯片都出现 Ending address is not in module or is less than starting address 的错误提示。不知是哪里出了问题。

0 项奖励
回复
1 回复

1,562 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi 华 张 

CyclonePro is P&E product, I suggest you contact P&E for its usage. 

PEmicro | Experts in Embedded tools for Flash Programming and Development 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复