CW10.7 debug error:no creating session

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW10.7 debug error:no creating session

4,018 Views
josewu
Contributor I

My programming working environment is :CodeWarrior 10.7+Multilink ,the board is FXTH870911,my PC is Window 7(32 bit)

the project compile OK,but cannot launch debug file(stop at 61%).the error show:no creating session.So ,how can i slove this problem.Thank you

0 Kudos
Reply
1 Reply

3,886 Views
david_diaz
NXP Employee
NXP Employee

Hello Jose,

I hope all is great with you.

Please review the file attached to this response. I recommend reading the Programming the device section in which detailed information is shown regarding the debug session.

Usually, the problem is solved with the following instruction:

pastedImage_1.png

I hope this information helps.

Regards,

David

0 Kudos
Reply