CW10.7 debug error:no creating session

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW10.7 debug error:no creating session

3,772件の閲覧回数
josewu
Contributor I

My programming working environment is :CodeWarrior 10.7+Multilink ,the board is FXTH870911,my PC is Window 7(32 bit)

the project compile OK,but cannot launch debug file(stop at 61%).the error show:no creating session.So ,how can i slove this problem.Thank you

0 件の賞賛
返信
1 返信

3,640件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello Jose,

I hope all is great with you.

Please review the file attached to this response. I recommend reading the Programming the device section in which detailed information is shown regarding the debug session.

Usually, the problem is solved with the following instruction:

pastedImage_1.png

I hope this information helps.

Regards,

David

0 件の賞賛
返信