CW, Hierarchy problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW, Hierarchy problem

1,530 Views
louishdy
Contributor II

Hello,

 

I am a beginner with Code Warrior for my internship. I have problem when I load my project. It said that there is a problem with the hierarchy. Then, a new folder "Rescued Items" is created with some files (which had this problem).

 

Furthermore, some files are duplicated: when i chekched their path, they are from another project (the original one). Is it a problem with my makefile?

 

Thank you for you help.

Labels (1)
0 Kudos
Reply
1 Reply

1,417 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Louis

For the problem of ‘Rescued Items’, please refer to this link, and review its attached doc < Rescued Items Whitepaper.doc>:

Codewarrior does not load the .lib file.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply